Before you export a project
If you are exporting a project for the first time to the Power Operation project, you need to create a matching project in Power Operation. To do this:
- In Power Operation Studio: Click Projects, add a new project. Be sure that the Template Resolution is SXGA.
 - Add your project to the Profile Editor, ensuring that the name matches exactly the one that you added in Power Operation Studio (to ensure that it correctly exports to its matching project).
 
If you have questions about any of the fields, click Help.